EIP.MISSEDPACKETCOUNT
Description
The internal counter used to trigger F7005 Cyclic Setpoints Missing fault. The counter increments by 3 on every missed cyclic packet and decrements by 1 when a packet is received.
Examples
The following chart provides an example of how the fault counter behaves using the default threshold of 9:
|
Fieldbus Cycle |
Packet Received |
Counter |
Faulted |
|---|---|---|---|
|
0 |
Yes |
0 |
No |
|
1 |
Yes |
0 |
No |
|
2 |
No |
3 |
No |
|
3 |
Yes |
2 |
No |
|
4 |
Yes |
1 |
No |
|
5 |
No |
4 |
No |
|
6 |
No |
7 |
No |
|
7 |
Yes |
6 |
No |
|
8 |
No |
9 |
Yes |
|
9 |
Yes |
8 |
Yes |
|
10 |
Yes |
7 |
Yes |
|
11 |
Yes |
6 |
Yes |
Context
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-10-04-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 (disabled) to 216 |
|
Default Value |
9 |
|
Data Type |
Integer |
|
Stored in Non-Volatile Memory |
No |
Variants Supported
EtherNet/IP drives: AKD2G-SPI
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
3903 |
1 |
3903 (0xf3f) |
EIP.MISSEDPACKETCOUNT |
Unsigned16 |
Read Only |
Yes |